Part Number: LMX2594 Hello,
We've seen an issue in roughly 13% of units where we do not get any RF output at the low end of the temperature range (-40 C) on LMX2594. In units we see fail, we typically have to increase temperature by about 10 degrees…
Part Number: THS4535 Other Parts Discussed in Thread: THS4561 , Dear Technical Support Team,
I have simulated SE to DIFF with TINA TI.
Attached file is my configuration and result of output.
THS4535 TINA-TI SEtoDIFF.TSC
THS4561 has wide supply…
Hi Peng,
HWA memory bank that stores compression paramset output is not used by any other paramset when you use fast range processing option. I think you are using 4.7.0.1 or 4.6.1.2 SDK. In these SDK versions, fast range processing option has a single…
Hi Tim,
I generate config file from mmWave Demo visualizer for the same Max Range, RangeRateResolution and RangeResolution. I compared this config file with the one generated from sensing estimator and I see the below differences.
left side : config…
Hi Jeff,
The jitter looks fine from the waveforms you shared; from my estimation it should be in range of 376kHz to 424kHz, for a 400kHz part. But it would be clearer if you can share the time stamps between the starting and ending edges, also the edges…
Hi Praveen, Sorry for the delay in response.
Praveen Jeevanantham said: Does the 1D sensing demo send range data over UART by default?
Yes.
Praveen Jeevanantham said: Is there any documentation for the UART data format (TLV structure)?
Sure, the…
JiaQuan Zhao said: and, what is your mentioned equation above?
Is it this one?
Yes this is the equation I'm referencing.
JiaQuan Zhao said: I'm curious, what theory or literature do you base to conclude this conclusion?
I am hesitant to say…
Part Number: MCF8329A Hi TI,
The data retention of the configuration data in the EEPROM of the component is specified as 10 years within the temperature range of -40°C to 150°C . This value corresponds to what number of write cycles?
For example,…
Part Number: MSPM0G3507 Subject: MSPM0G3507SRG Qualification for −55°C to +125°C Operation (-EP Variant)
Hello TI Team,
We are evaluating the MSPM0G3507SRG family for use in an application requiring an operating temperature range of −55°C to +125…