Hi Manoraj,
Manoraj Selvaraj said: but there is a limitation in the slave device that
To read complete FIFO, i need to read 7 register individually for number of configured sampling.
I am not aware of this slave device completely.
If there is a limitation…
Part Number: CC2530
Tool/software:
The example code for the CC2530 (SWRC135B.zip) has the following code for transmitting a frame.
uint8 halRfTransmit(void) { uint8 status;
ISTXON(); // Sending
// Waiting for transmission to finish while(!(RFIRQF1 & IRQ_TXDONE…
Part Number: TLV320DAC32 Other Parts Discussed in Thread: TLV320DAC3100 Tool/software:
Hi,
We are using a PDM microphone to capture audio, which is then processed in an STM32 microcontroller and sent to a DAC (TLV320DAC32). The DAC is connected to a…
Hi Wayne,
Wayne Huang said: Would you please elaborate what these three modes mean and what the difference is among them?
AES_OPMODE_GCM_HLY0ZERO - Galois/counter mode with GHASH with H loaded, Y0-encrypted forced to zero and counter is not enabled.
AE…
Part Number: IWRL1432 Tool/software: Hi Expert,
In TI Industrial toolkit Bike radar example, it provide IWRL1432 pre-build image only, when TI will provide source code?
dev.ti.com/.../node
Thanks
Daniel
Part Number: DS90UB960-Q1 Tool/software: Hi team,
For 4*UB935>>UB960 application, what is the example code for basic synchronized CSI-2 forwarding? I think below example code is for 4*UB933>>UB960, thanks!
BR
Jiawei