Part Number: DRV8334 Other Parts Discussed in Thread: CSD88599Q5DC Tool/software: Hello,
I am having an issue using the DRV8334 to drive an external H-bridge for a brushed DC motor.
The DRV8334 is connected and routed to a TMS320F28P550SJ9PZ microcontroller…
Hi again,
Strange thing is here: FPC only need 20ms after power on. But our SW wait for 300ms after power on.
This means SCL stuck happened and continue to 700ms and then recovered.
So if you are suggesting we add a FPC402 reset(not port) after…
Part Number: AM625 On our TQMa62xx SoM, we've observed the I2C controller becoming stuck under high system load (simultaneous stress test of CPU, RAM and various peripherals). We've noticed multiple symptoms of this state:
SCL is permanently pulled…
Hi Liming,
Glad you were able to mitigate the issue.
Unfortunately, there are not any additional hidden registers that could help indicate this status.
You could check the "Port SCL Stuck Interrupt Register" and "Port SDA Stuck Interrupt Register…
Part Number: BQ76952 Tool/software: Hello TI Community, I'm experiencing an issue with the BQ76952 IC in my project where the SDA line is stuck low while the SCL line remains high. This happens during field operations, and I'm unable to get back to normal…
Part Number: BQ76952 Other Parts Discussed in Thread: BQ34Z100-R2 , TCA9416 , Tool/software:
We’re using the BQ7695202PFBR in our design and observed something unexpected during power-up. Using a logic analyzer (Saleae), we’ve captured the SCL line…
Part Number: MSPM0G3507 Tool/software: Hi champs,
I am asking this for our customer.
The user uses I2C as target mode to implement PMBus 1.2.
When the I2C SCL is held low abnormally, how does the user know and then reset I2C module?
For example…
Part Number: MSP430FR5738 Hi,
We are having an issue where sometimes the msp stops replying correctly on the i2c until it gets reset.
The msp acts as slave.
When it starts to misbehave, the msp acknowledges the address, the data received, but…
Part Number: TCA9617A Other Parts Discussed in Thread: TCA9803 , , TCA9517A , TCA9517 , TCA9511A , TCA4307 Tool/software: Hi Teams,
How to Optimize Pedestal with SDA Low Level?
Hello Carl,
If the 3V3_i power is always on, then then the temperature should be constantly on and can constantly receive THERM Status. There is not a setting that would cause the THERM2 output to get stuck low. I do not see an issue with turning off…