Hi Ravichandra,
Below is a example of how to use commands via I2C to change data flash parameters found in the bq27530 Technical Reference Manual:
/cfs-file/__key/communityserver-discussions-components-files/196/8037.bq27530_2D00_G1-SLUUA73-TRM…
Dear Sir,
My customer want to use Sony's ISX017 CMOS sensor for their Car Cam project. Do you think they can use DS90UB913A with it? It's parallel output interface is 16bit YCbCr. Thanks for your kindly help.
Or they have to choose another FPD-Link…
Hello Kailyn,
I am sorry that you have problem with read/write to the registers. Can you give me the registers value of FEh and FFh? Those registers is used for selecting read/write to which decoders (TVP5154 has 4 decoders). I also attached the TVP5154…
Hi Jwan,
Thank you for the correction regarding the temperature units; most often we are dealing with Celsius temperatures, and not Fahrenheit so I overlooked that point. Even if the temperature is in the expected range, I do suggest you check the circuit…
Part Number: AM62A7 Tool/software: Hello TI team,
We met issue about MIPI CSI Virtual Chancel preview on TI platform.
Our environment is as following:
TI SDK BSP version: V09_00_02
Linux version: 6.1.80
Device tree overlay setting…
Hi Sundar,
Please see the following attachments.
The first one is for the formatter board.
2514132E_dlpc120_formatter.pdf
The second one is for the DMD interface board.
2514103C_S450_DMD_ESD.pdf
Thanks,
Alex Chan
Hi All,
I am having difficulty getting this camera setup with the code and patch supplied by Leopard. I believe I finally have the kernel patched like they wanted it, but the LSP has changed since Leopard built the patch, so I ended up doing it by…
Part Number: DLP2010 Other Parts Discussed in Thread: DLPC3430 How do I change the Swap configuration , as seen in Table 9 in the attached document. Is this done using an I2C transaction? I cannot find an appropriate transaction in the Programmer's Guide…
Part Number: LP-MSP430FR2476 Other Parts Discussed in Thread: MSP430FR2476 I'm trying to set up an I2C connection where a VL6180X-SATEL is the slave device with the master device being the MSP430FR2476. From what I've read from design documents I believe…
Part Number: WL1837MOD Hello,
We are currently using a Varasite Som that uses the WL1837MOD with a Laird antenna nano blade antenna (MAF94355). We are in the process of adapting the same SOM to another one of our products but due do placement we need…