Hi Mitesh,
Mitesh Hiran said: Hello, I am trying to install/add soundtouch plugins of gstreamer in the SDK v9 but I get syntax error for PACKAGECONFIG_append_pn-gstreamer1.0-plugins-bad
Added the following line in the conf/local.conf file:
PACKAGECONFIG_append_pn…
I tried with an example from the SDK and I see the same issue with SysConfig 1.20. SysConfig 1.19 (and earlier) works.
Nathan Vander Wilt said: But how do I use it?
Go to your project settings. In the General -> Products tab, see if there is a SysConfig…
Part Number: LAUNCHCC3235MOD It looks like the mac os version of the SDK is missing from the list of downloads. Ver 6 has a Mac version, and the release notes for ver 7 say mac OS X is a supported OS.
Having a mac os version will help our development.…
Part Number: SIMPLELINK-CC13XX-CC26XX-SDK Other Parts Discussed in Thread: CC2560 , CC2650 , SYSCONFIG , UNIFLASH Dear team
I have two Launchpads: the first is CC2650 and the second is CC1352P7-4. For the CC2560, I used CCS 7.4, and for the CC1352P7-4, I…
Part Number: PROCESSOR-SDK-AM62A Hey there,
I'm trying to deploy a face detection tflite model on AM62A using TIDL-OSRT . The two outputs of my model are the score of face existence in the image and 6 approximate facial keypoint coordinates plus facial…
Reese Grimsley said: I was also under the impression SYSFW is backwards compatible such that these errors you're seeing are not expected. If you'd like to stick with the 9.1 SDK, could you supply more information about the errors you are seeing during…
Part Number: SIMPLELINK-CC32XX-SDK I am trying to port CC32xx Sdk from freertos to threadX, we managed to cross the compilation stage, while running we came across an issue, while debugging we found that in main() the board_init() function is called,…
Part Number: PROCESSOR-SDK-AM62A Hey there,
I'm trying to deploy a face detection tflite model on AM62A. The two outputs of my model are the score of face existence in the image and 6 approximate facial keypoint coordinates plus facial bounding box…
Part Number: PROCESSOR-SDK-J721S2 Hi Team TI,
I am working on Object detection application and I need to have control on dataset by enabling required datasets as per my project requires.
For this, I am analyzing "tidl_net_peele_300.bin" model which is…