Part Number: SN65LVDS386 Other Parts Discussed in Thread: SN65LVDS387 Hi Experts
I have chosen SN65LVDS386/387(16 ch) for LVDS to LVTTL & vice versa. For initial testing purpose i have connected IC (LVDS386) with single channel LVDS i/p-1st & 2nd pin…
Part Number: SN65LVDS386 Hi dear expert,
I have a question regarding to digital input pin level, in datasheet, it lists: high level input voltage and low level input voltage.
This spec is for all digital pin, including ENA/B/C/D signal and all differential…
Part Number: SN65LVDS386 I went through the datasheet for SN65LVDS386 IC package 64 Pin. I am unable to get the details. Can you provide me the details of it.
Part Number: SN65LVDS386 Other Parts Discussed in Thread: SN65MLVD048 Hi,
SN65LVDS386 is having internal pull for fail safe mode. If inputs are not connected, output will be in high state.
But as per my system requirements, if input is not connected(floating…
Part Number: SN65LVDS386 The datasheet for this device claims 250Mbps throughput. It is unclear whether that spec is per channel or the entire device. Please clarify
Hi Bravos,
The LVTTL outputs are not 50 ohms. Please see the equivalent input/output schematic diagrams on page 18 of the datasheet:
www.ti.com/.../sn65lvds386.pdf
Regards,
I.K.
Hi Boris,
I have included a screen capture from the data sheet of the SN65LVDS386 running at 250MHz. It shows an open eye at this speed so the consequence of moving to a higher data rate will be a somewhat smaller eye opening. How much that eye will close…
Other Parts Discussed in Thread: SN75LVDS390 , SN65LVDS390 , ADS5281 , SN65LVDS386 hello ,
Can anyone help me on this one ?
I have an ADS528x which has sampling rate of 50msps .... so i want convert th lvds ouput of adc to LVTTL/CMOS outputs ... ehich one…