Part Number: SN74AHC125-Q1 Hello team,
I have a question about delay time for SN74AHC125-Q1.
The tPLH and tpHL variation range on the switching characteristics looks same. Does it mean both of them can be varied to the same direction? I would like to expect…
The SN75173 has TTL outputs (see figure 7-1), so it violates the V IH specfication of the TXB0104-Q1. (But in this case, the inputs appear to work anyway.)
The TXB0104-Q1's output have a drive strength of only 20 µA. Your schematic does not show the load…
Part Number: TXS0104E Other Parts Discussed in Thread: TXU0104 , SN74AHC125 Please suggest a good level translator for translating 5V encoder logic signals to 3v3 logic, which supports all high resolution CPR encoders
TXS0104EDR can this part be used? …
Part Number: SN74AHC125 I have a customer with BAE Systems asking about the maximum Vol they would see if the device loading was 6mA with 3.3 Vcc. This would be over the entire temperature range of the part. There are no charts or specifications showing…
Part Number: SN74AHC125-Q1 Team, Are the below parameters something that we can provide?
-Thermal expansion: en.wikipedia.org/.../Thermal_expansion CTE1 [ppm] CTE2 [ppm] -glass-transition temperature: en.wikipedia.org/.../Glass_transition Tg [°C] Thanks…
Part Number: SN74AHC125-Q1 Other Parts Discussed in Thread: TLC555-Q1 Dear,
We need to perform a low cycle fatigue analysis for each component on our control unit and for that we need the Tg, CTE1 & CTE2 of the mold compound.
Is it possible to receive…
Part Number: SN74AHC157 Other Parts Discussed in Thread: SN74AHC125 Hi,
Need IBIS model for signal integrity analysis. Please advise if IBIS model of SN74AHC157 can be provided. Thanks.
Part Number: SN74AVC4T245 Other Parts Discussed in Thread: SN74LVC125A , SN74AHC125 , SN74LV125A
Hi team
There is a good new that we DIN sn74avc4t245rsvr !
Please help confirm the SCH is ok?