Part Number: SN74AUC1G04 Dear team
Does the VCC of PIN5 only supply IC power? Or must it correspond to the signal voltage of PIN2?
If SW_CTRL_N is a 3.3V signal, will it be a problem if VCC is connected to 1.8V?
Many thanks
Denny
Part Number: SN74AUC1G04 Other Parts Discussed in Thread: SN74AUC1G14-EP Hello support team,
we have an application with 1.8V logic level where speed (or more precise: low variation in propagation delay) is important.
Therefore I have chosen SN74AUC1G…
"Data retention only" means that the device works correctly as long as it does not need to react to any input changing or need to switch any output. When starting up, it is possible that the internal state is not the same as that demanded by the input…
Regarding the question:
"Thank you. Last question I believe. The FET TEST pin appears to disable TCK/TMS/TDI. Is there a scenario that this is done for specifically?"
No this does not appear to be done or needed on the JTAG emulator or on…
Part Number: SN74LVC1G04 Other Parts Discussed in Thread: SN74AUC1G04 Hello Expert,
My case is locked.
https://e2e.ti.com/support/logic-group/logic/f/logic-forum/999056/inquiry-about-single-inverter-gate/3691150
So I create new thread.
I want to get your…
Part Number: RF430FRL152H Other Parts Discussed in Thread: MSP-FET , Hi Experts,
Our customer is trying to program the RF430FRL152H chip by its EVM JTAG schematic but wonders if the power3V3 is needed He came across a question in the forum saying that is …
Other Parts Discussed in Thread: SN74LVC1G04 , SN74AUC1G04 Hello Expert,
I'm looking for Single Inverter Gate to support frequency range from 150MHz to 200MHz.
Could you give me available part?
Best Regards,
Michael
Part Number: SN74LVC2T45 Other Parts Discussed in Thread: SN65LVDS31 , SN65LVDS33 , SN74LVC2G04 , SN74LVC1G79 , SN74AUC1G04 , SN74HCS74 Good morning,
I have a question regarding calculating the maximum operating frequency for a non clocked device.
A TI rule…