Part Number: MAX3221E Other Parts Discussed in Thread: TS5A23157 , SN74AUP1G08 , SN74AHC1G08 Hi,
I needed a RS-232 transceiver having 2 UART IO and 1 RS-232 IO, Does TI have such IC?
Thanks
Part Number: SN74AUP1G08 Other Parts Discussed in Thread: SN74LVC1G08 , SN74AUC1G08 Hi Team,
My customer is asking is there's any description in d/s or info about output pin Y(pin 4)'s sink current data ?
I had check with d/s, not sure if IOH mean…
Part Number: SN74AUP1G08-Q1 Other Parts Discussed in Thread: SN74AUP1G08 Dear team,
Could you help to figure out what's different between SN74AUP1G08 I and SN74AUP1G08 Q ?
According to datasheet, it's the same package. But one have to "call TI", the other…
Part Number: SN74AUP1G08-Q1 Hi,
In customer application, there could be a scenario that Vi>Vcc (e.g. Vi=3.3V and Vcc=0V) We understand that the chip is not functioning under such scenario, but we would like to confirm it would not damage the chip or…
Part Number: SN74AUP1G08 Other Parts Discussed in Thread: SN74AUP1T08 What are the differences between the SN74AUP1 G 08 and SN74AUP1 T 08? According to their respective datasheets, both devices appear to be interchangeable. However, the input voltage requirements…
Hi Clemens-san,
Thank you for your reply.
Clemens Ladisch said: When using an external oscillator, a digital signal with rail-to-rail voltage would work fine.
The customer is thinking of using an external oscillator. Am I correct in understanding that the…
Part Number: SN74AUP1G08 Other Parts Discussed in Thread: SN74AUP1G17 , SN74AUP1G57 , SN74LVC2G17 Hi,
We see the max input rise/fall rate is 200nS/V in datasheet. NOrmally 20uS/0V~3.3V should beover our spec, but customer said it's still working ell on…
Part Number: SN74AUP1G08 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models The links to the IBIS models appear to be broken.
I am searching for the SN74AUP1G08, but the link here fails to download the model:
http://www.ti…
1. All plain CMOS inputs have such a limit. See [FAQ] How does a slow or floating input affect a CMOS device?
2. Slow inputs can lead to oscillations at the output, or damage.
3. The input rise/fall rate requirements are stricter for devices that a both…