Is there a more complete model for this? Since the IC is bidirectional, I would like to use the IBIS Model as an Output as well. Is there a model that hasn't been uploaded yet?
Other Parts Discussed in Thread: SN74CB3T16211 I have a customer who is looking to do the following: utilize voltage isolation in such a way to power the cpu driving the data bus and address bus without powering the SD Ram and USB. Note that he does not want…
Other Parts Discussed in Thread: SN74CB3T16211 Is 3.3V pullup required in CB3T family of devices (sn74cb3t16211 - 24 bit). we are using this device with VCC of 3.3V to translate 5V swing signals to 3.3v swing signals on a CPCI interface. In fact, the input…
Other Parts Discussed in Thread: SN74CB3T16211 , PCI2050B Hi,
I want to interface PCI2050B Bridge's secondary PCI bus with Virtex 6 FPGA that will support only 2.5V IOs. The PCI target logic will be implemented in FPGA. The problem is how to interface…
Other Parts Discussed in Thread: SN74CB3T16211 , SN74CB3Q16211 Hi,
We have used a SN74CB3T16211 in our design.
We basically want to shift 5V input to 3.3V output.
But due to the unavailability of the above chip (BGA version),
we are thinking to use…
Other Parts Discussed in Thread: SN74CB3T16211 Hi,
I am looking for a 16-bit digital bus switch which does level translation from 5V to 3.3V and uses 3.3V Vcc.
I was able to find a 24-bit bus switch (SN74CB3T16211) with the same specs but I want to…
I'm sorry for the delay.
Are you refering to the SN74CB3T16211? it looks like they are currently available from both digikey and newark.
An alternate suggest would depend on your application and max frequency. The SN74ALVC164245 is one option.
Other Parts Discussed in Thread: HD3SS6126 , TUSB8041 , TUSB8020B Dear Sir/Madam/Miss,
Do HD3SS6126 chip support for 8:1 multiplexer (USB 3.0)? Since its only designed for 2:1/1:2, I'm wondering can I cascade it into 8:1.
Is that will be a problem in…