Part Number: SN74LV1T125 Other Parts Discussed in Thread: SN74LVC1G57 , SN74AHC1G125 , SN74LVC1G97 , SN74LVC1G99 , SN74LVC1G98 , SN74LVC1G125 , , SN74LVC1G58 , SN74LV1T34 , SN74AHCT1G125 , SN74LVC1T45 Hi, I have a micro-controller with only 3.3V tolerant inputs…
Part Number: DS26LS31C I am using DS26LS31C for driving high speed optocoupler which is on different board. Max cable length is 10ft and I have used twisted pair shielded cable. Max transfer rate required 1Mbit/sec. Environment is very noisy and hence…
Thank you , Clemens for your contribution .
Kuo ,
I am not qualified to comment on the NXPs part , however,the NXP has schmitt trigger action on the inputs according to the datasheet which is not the same as schmitt trigger inputs . The input transition…
Hey Cedrick,
Just got out of the lab, it appears that it is the logic kicking in at that time. In my runs I was able to get similar pulls of the OC line where the pull was varied from about 50ns to 80us depending on the resistance value. Unfortunately…
Other Parts Discussed in Thread: SN74LVC1G57 TMDSPLCKITV3 Schematic.pdf
Good day everyone,
From the schematic of the PLC TMDSPLCKIT-V3 (attached to this post) in page 3, there is a section circuit which is connected to the lines: Line-Azc and Line-N. Basically…
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage…