Part Number: SN74LVC2G66-Q1 Hi,
There are two questions for SN74LVC2G66-Q1,
1. We would like to use SN74LVC2G66-Q1 on UART interface(TX & RX), is it ok for that?
2. Can SN74LVC2G66-Q1 support to 250Kbit/s & 1Mbit/s?
UART to RS232: https://www.ti.com…
Part Number: SN74LVC2G66
Hi Team,
Our customer wants to check the failure mode for SN74LVC2G66 under instantaneous high voltage and pin to pin short, does it will have below phenomenon? Can you help to check them?
1. explosion
2. combustion
3. damage…
Part Number: SN74LVC1G3157 Other Parts Discussed in Thread: SN74CBTLV3257 , , SN74LVC2G66-Q1 Hello. Can we have the Pspice model of the SN74LVC1G3157 and SN74CBTLV3257 devices?
HSpice can not be used with Tina nor Pspice TI tool!!
Regards.
Part Number: SN74LVC2G66 Other Parts Discussed in Thread: TMUX1112 "My application (PCIe system) needs some flexibility in switching the SMBUS on and off to specific endpoints. To that end I’m using a SN74LVC2G66DCU Analog switch. This works for the clock…
Part Number: SN74LVC2G66 Other Parts Discussed in Thread: TS5A23166 Hi,
Will there be reverse current when the VCC is 0V in SN74LVC2G66?
My test result from the lab shows that some times side B will short and some times doesn’t.
May I confirm with…
Part Number: TXU0102 Other Parts Discussed in Thread: TCA9511A , LSF0102 , TCA9406 , PCA9306 , SN74LVC2G66 , TXS0102 , TCA9803 Hi team,
I'd like to know if VCCA and VCCB of TXU0102 can be same voltage and this device can be used as ON/OFF switch for I2C.…
Part Number: SN74LVC2G66 Hi Team,
We understand that ICC is 10uA(max) at VCC=5.5V, TA=-40℃ to 85℃ and ICC is 1uA(max) at VCC=5.5V, TA=25℃.
However, we would like to know about ICC value at VCC=1.9V, 3.8V, 5.0V and TA=-10℃ to 40℃.
Could you please let…
Part Number: SN74LVC2G66 Hello team ,
Can i used SN74LVC2G66 for I2c data line ?
i am asking because my i2c is open drain configuration with weak pullups to the 3.3V supply line .
Part Number: LSF0204-Q1 Other Parts Discussed in Thread: SN74LVC2G66-Q1 , TCA9517-Q1 , SN74LVC2G17-Q1 Can we use this part as buffer, by connecting Vref_A and Vref_B at the same voltage level?