Part Number: SN74LVC3G34 Hello,
I am using the SN74LVC3G34 buffer to connect an SPI bus to a RAM.
What I am observing is that the buffer output signals decrease over time, which causes the RAM to fail when processing the data. I have tried different…
Part Number: SN74LVC3G34 Other Parts Discussed in Thread: SN74LVC2G17 , UCC27517 , SN55451B , SN75451B , UCC27517A-Q1
Hello,
I am using the buffer to drive optical transmitter which can require a current upto 96mA in worst case. As per the datasheet…
Hello,
In addition to the recommendation above, there is a newly released device that is optimized for SPI buffering or level shifting:
https://www.ti.com/product/TXU0304
https://www.ti.com/product/TXU0304-Q1
It can support 1.1 to 5.5V supply…
Part Number: SN74LVC3G34 Hi,
I know that SN74LVC3G34 has Junction-to-ambient thermal resistance, but now the customer requests Junction-to-case thermal resistance. Do you have theta-JC for SN74LVC3G34? Or it should be OK if you have similar device functionally…
Part Number: SN74LVC3G34 Other Parts Discussed in Thread: SN74LVC3G17 Hi Sir,
Do we have schmitt trigger which is pin to pin compatible with SN74LVC3G34DCTR?
And the schmitt trigger can support SPI interface.
Thank you.
Part Number: SN74LV4T125 Other Parts Discussed in Thread: SN74LVC3G34 We use the following TI logic IC for driver on the board, And we need to check the minimum and maximum signal propagation delay times for each.
SN74LV4T125RGYR SN74LVC3G34DCUR
…
Hi Kelly,
Everything looks correct in the schematic for driving an LED with the SN74LVC3G34. I would recommend taking a close look at everything in the current loop for the LED -- how is the ground connected to the supply? Are there any weak connections…
Part Number: SN74LVC3G34 Hi,
Customer is using SN74LVC3G34DCTR with schematics as below now with R69=0Ohm, C55=0.01uF
They tried to measure input and output with waveform plots as below. You can see some oscillation at the output signal. The questions…