Part Number: SN75121 Hello,
My customer have some questions about thermal parameters for SN75121.
[Q]
Please tell me the following values in the NS package.
* TJmax (Maximum Operating Junction Temperature)
* Theta ja (Junction - Ambient Thermal…
Other Parts Discussed in Thread: SN75121 , SN75124 , SN75123 Hello,
according to the datasheet of the SN75121 (SLLS074C) the part is 'Not recommended for new design'.
So, my question is which is the replacement part for it?
Does the same apply to…
Other Parts Discussed in Thread: SN75121 , SN75124 We build new and maintain equipment designed in the 80s. There are several signals communicated with V/F and F/V 50KHz to 100KHz.. The signals are transmitted using SN75121 and received with SN75122 over…
Hi Naveen,
Do these parts need to be military grade?
I ask because the SN55121 is obsolete, but the SN75121 is still active and provides the same function.
The '244 function is very common. We have multiple families of parts that do this. I am…