Part Number: SN75LVDT1422 For this question, I am specifically referring to setup/hold violations associated with the TA[6:0] and TB[6:0] pins (parallel inputs).
I have an application that uses a bank of SN75LVDT1422 devices to transmit data from a parallel…
Part Number: SN75LVDT1422 Can only the A channel of this part be used to pass 7 bits of data over the TA+ / TA- , RA+ / RA-, with the TCLK + / TCLK - and RCLK+/ RCLK- and not have the TB+/ TB- and RB+ / RB- pairs connected between the chips? In my application…
Other Parts Discussed in Thread: SN75LVDT1422 Hi,
I am interested to use SN75LVDT1422 to serialize a set of parallel data which are in 5V TTL.
In the datasheet, it says that SN75LVDT1422 accepts 14 TTL input lines and generate 2 LVDS streams. But the…
Other Parts Discussed in Thread: SN75LVDT1422 Customer wants to know how to use the SN75LVDT1422 or other SERDES to drive long distance CAT-5 cable less than 10m at 100Mbps to 300 Mbps max. Needs an EVM if it available
Other Parts Discussed in Thread: SN75LVDT1422 Can the SN75LVDT1422 SERDES operate with a burst clock (see customer inquiry, below)?
Will the PLL achieve a faster lock if the clock burst off ime is under the typical PLL lock time?
Customer's Applicatio…
Hi Fajar,
The SN75LVDT1422 has 14 pins on its parallel interface and it can operate with a reference clock from 10-100MHz. I have some other recommendations with larger parallel interfaces but they require a minimum clock frequency of 20MHz, will that…