Part Number: SOT23-UNIV-AMP-EVM Other Parts Discussed in Thread: LMV321-N I am confused about the frequency for the PWM signal coming in. It is between 0 and 3.3 V. The C1 and R1 form a low pass filter. Which I calculated to be 33 Hz, so I thought I''l…
Part Number: TAS5825MEVM Other Parts Discussed in Thread: TAS5822M Hi!
I am looking for a stereo power amp / speaker amp EVM that can take a digital audio input from a USB cable, connected to a Linux PC.
Actually the purpose of the stereo amp is to deliver…
Part Number: LMP7715 Hi Team,
My customer requests for EVB for LMP7715MFX/NOPB (SOT23-5) and I'm confused with all packages types. Could you help?
(1) I'm looking at DIYAMP-SOT23-EVM . Is it available for SOT23 5-pin? The user's guide does not…
Part Number: SMALL-AMP-DIP-EVM Hi
Can you please provide the CE/EU Declaration of Conformity for SMALL-AMP-DIP-EVM?
This product appears to bear the CE-Marking but the EU D eclaration of Conformity is not available on the website.
Thank you
Other Parts Discussed in Thread: DUAL-DIYAMP-EVM , OPAMPEVM-SOT23 , OPAMPEVM-MSOPTSSOP Hi,
I have purchased
DIYAMP-SOIC-EVM DUAL-DIYAMP-EVM OPAMPEVM-SOT23 OPAMPEVM-MSOPTSSOP
I want to make stencils. Can I get gerber files for these evaluation modules?
Thanks…
Part Number: OPAMPEVM-SOT23 Other Parts Discussed in Thread: TL331 Hi Team,
My customer would like to try our OPA TL331BIDBVR, I see it’s SOT23-5 package and our EVM also have SOT23-5, but I am not sure why have SOT23-5A and SOT23-5B, may I know what’s…
Hi Katherine,
Besides TLV9062IDDFR, we have a bunch of devices available now for the same package:
TLV9052IDDFR: 5MHz, 15V/us high slew-rate, RRIO op amp.
TLV9002IDDFR: 1MHz, RRIO, 1.8V to 5.5V op amp for cost-optimized systems
LM358LVIDDFR/LM2904LVIDDFR…
Part Number: TI-PLABS-AMP-EVM
Dear Technical Support Team,
I have TI-PLABS-AMP-EVM, but I don't have virtualbench.
Which product number should I use with TI-PLABS-AMP-EVM.
I guess that VB-8012 is used for precision lab video. Is it correct?
https…
Hi Jacek,
We recommend using the PCM2912A instead of the PCM2912.The gain for the MIC amp is controller externally by the MAMP pin, Low = 0dB and High = 20dB. This device is an integrated USB codec that uses a standard USB streaming audio driver and all…
Hi,
Greetings. Our customer would like to have a copy of the gerber file of DIYAMP-SOT23-EVM. We would appreciate if you could provide us the gerber file. Thank you and have a nice day. Regards, Cedrick