Part Number: TAC5112 Hello team - can you please help with the below
We implemented the registry settings as described in section 8.1.2:
Question: These settings seem to detect the if a jack is connected at the OUT pins and not at the IN pins…
Part Number: TAC5112 Tool/software: Hi team,
My client is considering using the TAC5112 for a laptop project.
The application seems to have a Modern Standby feature, and they are concerned whether the TAC5112 can process audio data in that state.…
Part Number: TAC5112 Other Parts Discussed in Thread: TAD5112 , Tool/software: Hi TI support Team,
I am wondering what is different between TAD5112 and TAC5112.
thanks,
Part Number: TAC5112 Tool/software: Just to confirm regarding the output circuit:
Am I correct in understanding that a full low-pass reconstruction filter isn't required—just a simple RC filter on the differential outputs?
I'm currently having difficulty…
Part Number: TAC5112 Hi team,
I am evaluating the TAC5112 using the TAC5112 EVM and measuring the DAC analog output.
Test conditions: - Device: TAC5112 - Board: TAC5112 EVM (default settings) - Input: 1 kHz sine, fs = 48 kHz, 24‑bit (ASIO) - Output…
Part Number: TAC5112 Tool/software: HI,team
When is the full release of TAC5112 scheduled?
I heard that mass production will start in October, but this is still a preview.
Best regards,
Part Number: TAC5112 Other Parts Discussed in Thread: TAC5212 , INA217 , INA333 Tool/software:
Hello,
I’m currently working on interfacing both XLR and TRS inputs with the TAC5112 codec and would appreciate some clarification regarding the recommended…
Part Number: TAC5112 Hi team,
We are evaluating the TAC5112 (TAC5x1x family) and would like to use the device GPIO pins (e.g., GPIO1, GPIO2) as general‑purpose GPIOs that can be controlled from our Linux system (set as GPI/GPO and toggled/read from…
Part Number: TAC5112 Tool/software: Hi Team,
if we need echo cancellation for audio mic application, how will TAC5112 a stereo audio codec configured with a DSP to performs echo cancellation.
Thanks.
Part Number: TAC5112 Tool/software: Hi, We hope to mix ADC(CH1) input signal on DAC(CH1) with a certain gain.And in the data sheet,Fig 7-1. Functional Block Diagram(P-21/177), there are feed back loops before ADC to after DAC. In addition Fig.7-17. ADC…