Part Number: TAS5614 Hi,Team
The customer is currently using Tas5534+Tas5614, there are 2 problems as follows, (AMP power supply voltage: 25V, load 4 ohms) 1: When the input is -24db, there is 2.6% distortion measured at the speaker end, and the output…
Part Number: TAS5614LA Other Parts Discussed in Thread: TAS5624 , TAS5614 , TAS5548 , TAS5538 Hello Now we need to select the audio amplifier to drive the 3ohms/120W loudspeaker in our subwoofer, we want to use the structure of"5.8G wireless module + PWM…
Part Number: TAS3251 Other Parts Discussed in Thread: TAS5614 Hello There are two solution for the subwoofer of our soundbar; 1):5.8G wireless module +TAS3251 + Loudspeaker(subwoofer) 2): 5.8G wireless module +TAS5534 + TAS5614 + Loudspeaker(subwoofer…
Part Number: TAS5614 According to the specification of this IC (TAS 5614), the recommended load impedance in BTL mode is Minimum 3 ohm. I want to use it at 2.5 Ohm, but can I use if I take care the peak current ? In my plan, the peak current is 11 A. In the…
Part Number: TAS5614 Hi Sirs, Would you pls advise the Tc temperature specifications of the TAS5534 and TAS5614 devices per customer's request? Thank you and Best regards, Wayne Chen 08/16/2018
Part Number: TAS5614 Hello,
I'm currently using the TAS5614LA in a design with all 3 mode pins set low, so configured as 2 x BTL with differential input PWM. At a basic level, the device works, but recently when I've been looking for greater precision…
Part Number: TAS5614 Other Parts Discussed in Thread: TAS5538 Hi TI,
In our factory, we need to read TAS5534 ID from register which is constant value to check TAS5534 IC is available or not.
I have checked the datasheet of TAS5534, there is 0x01(General…
Part Number: TAS5614
Hi TI,
We have requirement for bypass TASS5534 control. Please see below
During wired mode, we want to apply bq settings of upper TAS instead of lower one.
So we need to bypass the biqaud settings for lower TAS5534.
How to enable…
Downey,
Yes, from easier technical support perspective, TAS5614 would be recommended.
While if there is other considerations like cost impact or sourcing side, TAS5432A can still be used.
Dylan