Part Number: TCA6424 Other Parts Discussed in Thread: , PCA9539 , TCA9539 Tool/software: Hi,
Do I need any special drivers (controls) to use TCA6424 under Linax?
Best Regards,
Nishie
Part Number: AM62A7 Other Parts Discussed in Thread: TCA6424 Tool/software: HI TI
can't set TCA6424 CSI_GPIO0 to 1
device tree:
include <dt-bindings/gpio/gpio.h>
&{/} {
clk_imx728_fixed: imx728-xclk {
compatible = "fixed…
Part Number: SK-AM62 Other Parts Discussed in Thread: TCA6424 , Tool/software: Hi, Dear Expert
The goal of this thread is try to let "uart1" of M.2 slots real inter-connect to AM62x uart1 (A18/B19/E19/A20)
So we need try to study how does TCA6424…
Hello Nirojan,
Nirojan Navaratnarajah said: From our side we tried to initialize the I2C driver and also created an instance of the IO expander using the driver from TI
Just to confirm here, were you using the drivers mentioned on this page: https://software…
Part Number: TCA6424 What is the purpose of the ADDR bit in the slave address, in other words, why are there multiple slave addresses provided? Does the ADDR bit mean that the slave responds to either slave address? I am only familiar with each I2C device…
Part Number: TCA6424
Hi Team,
Our customer design uses the TCA6424A. Due to delivery problems, they decided to use TCA6424 as an alternative based on the Errata of the datasheet.
However, they observed that the interrupt does not behave as with the previous…
Part Number: TCA6424
Hi,
We need to know what are the differences between PN TCA6424ARGJR and TCA6424RGJR.
The TCA6424ARGJR is an active device and the PN TCA6424RGJR is an obsolete item.
But are they interchangeable? We need to know if they have the…
Part Number: AM6422 Other Parts Discussed in Thread: TMDS64EVM , TCA6424 Tool/software: Hi experts:
I am using uboot2024.04 on TMDS64EVM board, the u-boot works well.
However,I have to transplant the uboot2024.04 to my new board.
The ethernet port 1 schematics…
Part Number: SK-AM62A-LP Other Parts Discussed in Thread: TCA6424 Tool/software:
hi
I am using AM62A-LP board
I have a question about the IO-Expender using the camera MIPI connector.
# SDK : ti-processor-sdk-linux-edgeai-am62a-evm-10_01_00_05
Please…
Part Number: TCA6424A Other Parts Discussed in Thread: TCA6424 Due to part shortages our buyer purchased TCA6424 parts where as all previous builds used the TCA6424A. Before we build these units what is the difference between the parts?
Kevin