Hi,
I am using AM3354 platform and running my system Linux 3.12 (SDK7). Find my ps, top, lsmod status and suggest me where it is going wrong.
Regards,
Anil
log-top-ps-lsmod.txt
Mem: 50892K used, 457504K free, 0K shrd, 2284K buff, 16036K cached…
Hi Yordan,
I am using custom board with using frame buffer, i am not using pvr driver by default.
Please find attached my system configuration with top command.
Still i am getting very slow with qt apps.
Regards,
Anil
7181.System-Cofiguration.…
Hi,
I am using 1GB nand (1024MiB, page size: 4096, OOB size: 224) in my am335x platform and trying to boot from NAND, it is running and my applications also running.
But problem is while booting at the beginning the continuously the below error messages…