Part Number: THS3091 I have a deisgn with 2 cascaded THS3091 amps and I'm at the layout stage of voiding out layers under the amp. I have attached pictures of my current plan--can you please verify that this is suitable or if not, let me know what I should…
Part Number: THS3091 Other Parts Discussed in Thread: TLV1872 , LM6171 Hi TI team,
I’m building a custom over-voltage protection (OVP) circuit for an AWG output (±10 V, 50 Ohm up to 500 MHz). For external signals , I only need the OVP detection to work…
Part Number: THS3491 Other Parts Discussed in Thread: THS3091 , We compared the THS3491 with THS3091 (latest die revision) and can not see any differences. Exactly the same board types for both.
We checked amplitudes with frequency-sweeps and step responses…
Part Number: THS3091 Other Parts Discussed in Thread: OPA692 , OPA3692 , THS7303 , THS7353 , THS7347 , THS7327 , THS7316 , THS7365 , THS7373 , THS7368 , THS7364 , THS7372 , THS7360 , THS7376 Tool/software: Hi i m designing a video splitter with 1 input…
Part Number: THS3091 Other Parts Discussed in Thread: THS3061 , , THS3491 I'm considering using the THS3091 or THS3061.
How do these two parts compare in regards to intermodulation distortion?
Is there a model/simulator that would allow simulation…
Part Number: THS3091 Tool/software: Dear TI Support Team,
With later batches of THS3091DDAR we measure a significant rise in slew rates . This changes the characteristics of our device .
I could not find any PCNs for this part.
As far as I could…
Part Number: THS3091 Tool/software: I connected a PWM GPIO to the input and connect the output to a 50R oscilloscope input:
When the PWM (70KHz) is falling done (falling edge from 3V3 to 0V), I have a 1V gap for 50nS. Do you know where it is coming…
Part Number: THS3091 Tool/software: Hi,
I am using a THS30911DDA to visualize a PWM from a GPIO to a BNC connected to a scope.
This componenet is supplied by a +/- 12V power supply.
The input signal is a square one with 70KHz frequency and a duty…