Part Number: THS3217
Hi!
Could you, please tell me, what i'm doing wrong?
There are graphs of HD2 and HD3 in the datasheet of ths3217 t. It's easy to see, that if a signal has amplitude about 2,5 V in the output of ths3217, there will be about…
Part Number: THS3217 Other Parts Discussed in Thread: LMH6401 ,
Hi!
I need to drive LMH6401 with THS3217 and get very low HD2 and HD3 (not worse as datasheet's one at +6V and -6V supplies)/
There is a graphic of HD2 and HD3 vs power supplies in datasheet…
Part Number: THS3217 Hello,
My customer is designing power trees for THS3217.
To keep the performances specified in the datasheet, any power rail ripple or noise requirements to be followed?
Best regards,
K.Hirano
Part Number: THS3217 Hi Team,
According to the THS3217 data sheet, the output stage of the device shows overshoot for a step response. My customer has a circuit that shows similar and they'd like to minimize the overshoot.
Here are some design requirements…
Part Number: THS3217EVM Other Parts Discussed in Thread: THS3215EVM , , THS3217 Hello, engineers: I would like to ask a question, in the application THS3215EVM and THS3217EVM (SBOU161A), I see a lot of test points are not directly added to the trace, but…
Part Number: THS3217 Hello Andrew, I was kind of cruising the questions on the parts I helped develop and introduce, the THS3217 being one of them, You are probably done with this issue by now, but just in case ---
Your issue was probably the C182 27pF…
Part Number: THS3217 Other Parts Discussed in Thread: DAC3283 , LMH5401
Hi, I am designing the interface circuit for current-sinking DAC3283 using THS3217. I went through the TI's application note and tried to design the circuit based on the topology…
Part Number: THS3217 Other Parts Discussed in Thread: TINA-TI Need a very fast differential amp such as THS3217.
I need to model my circuit & simulate its transient and ac response.
What model TINA-TI will correspond to THS3217 chip?
You can suggest…
Part Number: THS3217
Hello! Will there be any problem or effect in the chip's performance if the following resistor values were changed to 100ohms?
Thank you!