Part Number: THS4041-Q1 Other Parts Discussed in Thread: THS4041 , LM7171 , THS4061 , LM6171 Dear Team,
I am looking for a TI part replacement for Linear PN LT1363 , I found the replacement in TI website : THS4041-Q1
Can you please help me suggest if this…
Other Parts Discussed in Thread: LM7171 , LM7171QML-SP , LM7171QML , THS4041-Q1 , THS4041 Dear Members,
I am a searching for a single supply high speed OpAmps to drive a MOSFET Push-Pull Stage of an Inverter Gate Drive .
The OpAmps are to be configured in…
Hi Matthias,
The Iout of 65mA is for a single stage of THS4042, or each channel. If you run both amplifiers in parallel, you can create an amplifier with slightly less than a 130mA total output current, since you are using 9V supply instead of 10V. The…
Hi Kuo,
For the AD817 (+/-18V supplies, 350 V/us slew rate, good video performance, 50MHz, unlimited cap load, 7.5mA supply current), the closest device is the LM7171 (which is not really rated for "unlimited cap load" but might otherwise fit).…