Hello Steve,
There is also the THS4211, however it doesn't meet your voltage noise requirement. If that is okay with your system, that's another part to consider.
Thanks!
-Karan
Part Number: OPA858 Other Parts Discussed in Thread: THS4211 , , THS4215 Hello,
I am looking for a buffer (Analog) with the following requirements:
1) Input voltage range: 0V to 0.9V
2) Fq: ~100MHz to 200MHz
3) Iq, Noise: We don't really care about it…
Hi Hooman,
I would like to redesign the tranismpedance amplifier and use the unity-gain stable THS4211 instead of the LMH6629. I'd like to lay the board out for the SO-8 package simply because if the THS4211 doesn't work, there are several single op-amps…
Other Parts Discussed in Thread: OPA695 , THS3091 , THS4211 Hello all,
I am using THS4211D for pulse amplification and the input pules is 3.3V but Now I want to amplify 10V , I am using single supply configuration in my circuit,
Please suggest,
Regards…
Hi Hooman,
I don't think the OPA820 comes in the DGN (8 pin with thermal pad underneath) package. Is there another op-amp in the DGN package that would work?
The THS4211 has the slew rate and bandwidth I need but the voltage noise is high for my…
Hello Nishant, Unfortunately with the package style you have chosen, we don't have an alternate amplifier to be a drop-in replacement with higher bandwidth that also has JFET inputs. You can try using the THS4211 and THS4271 both of which have higher…
Hi,
Could it be because the "Calculate nodal voltages" function in the "AC analysis" option in the "Analysis" menu doesn't take into account the possibility of the circuit instability and resulting oscillations (there…
Other Parts Discussed in Thread: OPA847 , TINA-TI , OPA842 , OPA627 , THS3201 , THS4211 , THS4271 Hi guys,
I am designing an transimpedance amplifier with an diode capacitance for nearly 50pF, and the frequency would go up to 35MHz. I used the basic topology…
Liang,
J4 can be used in conjuction with J3 to provide a fully differential, DC coupled output. In order to do so, the transformer should be removed and resistors R20, R23, and R27 should be installed. J1 and J2 can be used similarly for channel B.
…