Part Number: TIDA-010071 Hi,
We were thinking of using TIDA-00637 for a project, but I see that TIDA-010071 has been released in 2019 whereas TIDA-00637 has been released in 2015.
Are there any circumstances under which we shouldn't use the latest design…
Part Number: TIDA-010071 Hi,
Any particular part number Ti Launch Pad recommended for this design ?
Also firmware files for same don't seem available for download.
Regards, JRock
Part Number: TIDA-010071 Hello,
I am working on TIDA-010071 for relay switching, But I`m not getting output power from the power supply section. I`m providing 230V AC i/p supply to the circuit.
I have used transformer 750344604(datasheet attached) to…
Part Number: TLV1805-Q1
Hi, Support Team
for AC charging Pile of control Pilot function, we reference J1772 EVSE Prototype and TI TIDA-010071
we choice TLV1850-Q1
ref :J1772 EVSE prototype
ref :TIDA-010071
our schematic have any concern?
if any suggestion…
Hello Bhardvaj, You can find a description of the differences between TIDA-00637 and TIDA-010071 in these previous e2e posts:
https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation-hardware-system…
Hello Kai, Thanks for quick response! Referring to TIDA-010071 TLV1805 circuit required isolation >=2.5kV on control Pilot OUT signal. Yeah, an optocoupler will work, if it full fill the requirement. Thanks
Part Number: TLV1805 hi team
my applicaiton is AC charging pile that refer to TIDA-010071 document . so using TLV1805 for Control Pilot Signal is our solution.
my question is
why is the different output(PIN1) V of TLV1805 between simulation and measurment…
Hello,
pls find my answers below:
a) yes, you can replace it with TLV1805. Actually, in TIDA-010071 we already used TLV1805.
b) for the GFCI test, you can pick up any CT from the shelf, but only need to make sure the max voltage drop on the burn resistor…
Part Number: ISO1212 Dear ,
In reference design TIDA-010071,
Why the R71 and R72 connected to D19 Pin4, but R75 and R76 connected to D20 pin3?
rEGARDS,
BARD
Hello Robert
First of all, thank you very much for your interest. I continue to work, too. I request some sample products to better understand your product range.
I start working on AC Level1 and Level 2 models as in the project with reference number…