Part Number: TIDA-01525 Tool/software: Dear Team,
Could you please provide the TINA simulation files of TIDA-01525
www.ti.com/.../tidudh4.pdf
Regards
HARI
Part Number: TIDA-01525
Tool/software:
Hello
I have done some simulations with the TIDA-01525 and found during a transient simulation that there is a delay between the input and the output of around 1.8us. I was wondering what the cause of this…
Part Number: TIDA-01525 Other Parts Discussed in Thread: DAC80508 Hi TI,
I have the same request.
The current range of TIDA-01525 is satisfactory, but I want to apply PVDD at least 15V (because the voltage of the load is high) Can you give me a guide…
Part Number: TIDA-01525 The TIDA-01525 device is useful for me, but I would like to modify the schematic to change the amplifiers & transistors to handle higher voltages. Do you have an editable version of the schematic in .SchDoc format (or other schematic…
Part Number: TIDA-01525 Other Parts Discussed in Thread: OPA2376 , OPA2189 , OPA2192 , CSD22206W , CSD23285F5 Hi team,
The figure is the voltage controlled current mirror circuit diagram of TIDA-01525.
I want to configure Rload be about 3.5V LED within…
Part Number: TIDA-01525 Other Parts Discussed in Thread: TLV9061 Hello,
Can I set the voltage to 400 Volts for this circuit. Of course, I will use the flyback converter for 400 volt DC. I need: 0-200mA adjustable current source for 400 Volts.
Part Number: DAC80508 Other Parts Discussed in Thread: TIDA-01525 , DAC80516 , DAC60096 , AMC60704 Dear Technical Support Team,
I need 0mA-150mA current output solution.
I find TIDA-01525. It seems standart solution with DAC and BJT (max 200mA). …
Hi Cooper,
To my knowledge, TI does not have a device that can output current of that magnitude. Generally, we recommend a precision DAC with a high-side or low-side current source.
https://www.ti.com/tool/TIDA-01525
Take a look at this reference…
Hi Arelone and Kai,
The biggest issue you will find in the bandwidth. 500kHz is difficult because 1Msample is pretty much the max on our fastest devices. You can look at a Howland current pump for the output or a current mirror as a high-side current…