Other Parts Discussed in Thread: TIDA-01590
Dear all,
I have TIDA-01590-E1 board.
If i power ON the board and the board id is shown in my laptop like "Throughput Pheri" then i can able to Pair and connect the device. But the data from the sensor…
Part Number: TIDA-01590 Other Parts Discussed in Thread: PCA9548A , INA260 , INA229 Hello,
We are looking for the current sense measurement solution for solar plants where voltage string is carry 1500V up to 30A.
This TIDA-01590 reference design seems…
Hello Carolus,
Can someone from TI, which worked on this reference design TIDA-01590, confirm us what should be creepage/clearance distance for transformer to satisfy 1500 V DC?
Used transformer 750316031 has 11mm min creepage and clearance distance…
Hi Guang,
I understand you concern regarding the 600Vdc being present on IN+ of INA195. My circuit use the similar technique as INA260 TIDA-01590 (see below). The INA260 has common mode range of 0-36V on the IN+ and IN- but still sees the 1200Vdc…
Part Number: INA302 Other Parts Discussed in Thread: TIDA-01590 , INA260 , TIDA-01065
Hi
I am designing 115VAC switch with mosfets(back-to-back configuration) and I want to measure load current with INA302A3. Can I use mosfet’s driver isolated ground…
Hello AnBer,
Thank you for reaching out on the forum. Could you tell us a little more about your DC DC converter (input, output voltages, and expected current levels, and what general topology are your customer is using). The INA260 shunt is not isolated…