Part Number: TL064 Hi,
I would like to know the value of Isink and Isource of TL 064.
What is the minimun value of Isink and Isource?
Best regards, Seishin
Hello,
a question regarding the minimum supply voltage came up, as there is no clear specification of it in the datasheet but on the product page there is.
product page states: 7V minimum required total supply voltage
but: in the datasheet there are graphs…
Other Parts Discussed in Thread: OPA4277 , TL064 Got good results for my project of EMG signal extraction by using TL064 to develop the Instrumentation amplifier coupled with the bias compensation. For enthusiasts needing more info. please post here, I…
Part Number: OPA4277 Other Parts Discussed in Thread: TLC2254 , TL064 , OPA4132 , OPA4188 Hi, support team
My customer has the questions as follow:
The supply voltage is ±5V. Input voltage is 3V pulse signal, duration of high level is 1.6ms and the…
Other Parts Discussed in Thread: TL062 En la figura 27 "IC Preamplifier" de dicha hoja de datos aparece un esquema usando el TL062. A primera vista aparentan estar invertidas las conexiones inversora y no inversora del operacional. Estoy en un error? Si…
Other Parts Discussed in Thread: TL064 Hello,
I have a TL064 powered with +/- 16.6V. The - Input is connected to GND, and the + input is connected through 12k Ohm to the output of another op-amp also powered with +/- 16.6V, so this input sees 16.6V regularly…
Hi Roger,
just wanted to simulate your circuit, but I'm unable to understand it. The schematic totally confuses me... :-)
But I can say this: If I use the TL064/74/84 I always use phase lead caps in the feedback loop of OPAmps. 10...22pF is usually…
Other Parts Discussed in Thread: TPS60403 , TL064 Hello
We are working on TPS60403 to generate -5V as per attached circuit. We have used this in two products as below:
1) The load is only to bias a single TL064 OPAMP, product layout is small (~90mmx80mm…
The INA333 circuit did work however the body offset was too high and hiding all the EMG signal strength. Hence we built an IA using TL064 with bias compensation. Also you can use the reference pin on INA333 for offset cancellation...but found it more…