Part Number: TL16C750E Other Parts Discussed in Thread: TL16C750 Hello,
While testing out our design using the TL16C750E, we came into an odd behavior.
We are using the component in RS485 mode so /DTR is our TX_EN and /RX_EN signal for the transceiver…
I have reviewed the datasheet regarding wetting this part into 64 byte FIFO mode. We are polling the part, and the baud is 115.2k, 1 start, no parity 2 stop, and 8 data.
Our code currently has LCR MSB=0 before these two writes to FCR:
FCR = 0xF1
1msec…
Other Parts Discussed in Thread: TL16C750 Hello,
I have a hardware which utilizes a TL16C750 for additional UART functionality. TL16C750 is connected to the emif bus of my DM368 processor. I actually have two questions:
1. The hardware designer has connected…
Other Parts Discussed in Thread: TL16C752D , TL16C750 Can you propose a similar part or solution like Exar - XR16C850? https://www.exar.com/ds/16c850-231-080905.pdf
Thanks.
Other Parts Discussed in Thread: TL16C750 How does the UART, in UART mode, indicate that all data, parity, and stop bits have been sent?
Do you have any timing charts on when the THR interrupt happens vs. the TX output when SCR TXEMPTYCTLIT is set to…
Hi,
The UART module is functionally compatible with the TL16C750 UART and is also functionally compatible to earlier designs, such as the TL16C550. You are correct that BCLK (which is 13x or 16x the actual baud rate) is used for syncing. Basically after…
There is a note in OMAP4 TRM in UART section:
"The UART is functionally compatible with the TL16C750 UART and earlier designs such as the TL16C550."
http://www.ti.com/product/tl16c750#feature
and it provides a link to next files,
http://www.ti…
Other Parts Discussed in Thread: TL16C750 Hi
I want to know the initialization of UART1 for polling tx/rx mode.
Awaiting for positive response.
initcode:
UART_SYSC =0X02;
while((UART_SYSS & 0X01) == 0X01);
UART_IER = 0x00; UART_MDR1 = 0x7…
Other Parts Discussed in Thread: NDKTCPIP , TL16C550C , TL16C750 , TL16C450 , TL16C554 , CCSTUDIO Hi,
I want to implement the flow control stuff on OMAP3703 Processor which has 16550 compatible uart driver.\
So antbody please give me steps to do this?
Thanks…
Other Parts Discussed in Thread: AM1705 , TL16C750 , AM1707 , OMAP-L137 I use a board based on the the EVM1707.
on my board:
- AM1705 CPU
- 32 MB SDRAM
- spi w25q32
-nand MT29F1G08ABADAWP
I`m using UART 2 port.
When I ported the bootloader, there was…