Part Number: TLE2061 Other Parts Discussed in Thread: OPA172 , TLV172 , OPA145 , OPA180 , OPA171 , , TLE2062 Hi,
Can you please suggest an alternate for TLE2061AM with much lesser open loop output impedance?
The quiescent current shall be equal to or less…
Part Number: TLE2061 Hello guys.
One of our customers wants to use TLE2061ID(Excalibur JFET-Input High-Output-Drive uPower Op Amps). But the device ESD perforemance data (HBM, CDM or MM) is not described in the device datasheet. They need the data to start…
Other Parts Discussed in Thread: TLE2061AM , TLE2061 , OPA2171 Hi,
I have an inverting amplifier based on TLE2061AM having gain of G=8. the input is 1 volt AC of 3Khz.Power supply is +/- 15V.
As per datasheet Figure 18, the Aol ~ 58dB @3Khz, 25degC &RL=10k…
Other Parts Discussed in Thread: TLE2061 , TLE2062 Hi,
As per datasheet the open-loop output impedance of TLE2061 and TLE2062 are 280 ohm and 560ohm respectively. But in TINA simulation I am getting open-loop output impedance as 140ohm. Can you please clarify…
Other Parts Discussed in Thread: TLE2061 , TLE2062 Hi,
As per datasheet the open loop impedance for TLE2061 and TLE2062 are different (280 and 560ohm), how to take care this change in Spice model from datasheet? For which device the spice model is provided…
Hi,
What is the test circuit used to evaluate VOM+ Maximum positive peak output voltage swing?
With RL=600ohm over full range temperature the VOM+ is 12V when Vcc is 15V. So output impedance of Opamp is 3V/20mA = 150ohm. Is this frequency & Gain dependent…
Hi Pengfei,
the OPA365 and OPA2365 need not to contain exact identical operational amplifiers. The TLE2061 and TLE2062 don't do that either, for instance. (They differ in the open loop output impedance.)
Looks like the OPA2365 limits to a lower short…
Hi Shihab,
provided the circuit is designed properly, the phase will not change very much in the range 1.26...2.75MHz.
I guess, this thread has to do with the TLE2061 from your other thread? Why not showing us a schematic?
Kai