Part Number: TLK106 Hello,
we are experiencing connection problems when the PHY is used in connections with Intel PHYs on the other side, also TP-Link devices fail with connection except the TLK106 is has auto-negotiation turned off. (Indeed, by probing…
Part Number: TLK106 Hello.
We are going to produce a series of devices with TLK106 onboard. The user of end equipment requests us to provide the MAC-addresses in advance. He's going to setup the gird infrastructure basing on this information.
Is there…
Part Number: TLK106 Hello,
TLK106 supports Auto-MDIX. It seems we can use cross cable or strait cable either because negotiation happens with link partner. Is my understanding about Auto-MDIX correct?
Best regards,
Toshihiro Watanabe
Part Number: TLK106 Hi,
We are using the 2 TLK106RHB PHYs in 2 different boards without RJ45 port/Cable.
Is it correct to connect the PHYs in below fashion:
MAC->PHY->Magnetics->Board to Board Connectors->Magnetics->PHY->MAC
The two MACs are…
Part Number: TLK106 Hi,
We are using the TLK106RHB PHY on the 2 separate boards and we are connecting them with some board to board connectors.
We are using the Magnetics near to the board to board connectors.
We want to know whether there is…
Part Number: TLK106 Hi,
Working with Phy TLK106L, we want to use it as full-duplex mode, the datasheet explain to force full-duplex mode with a 2.2kΩ pull up to AN_0 (led link), but our board design did not include this. So we want to force full-duplex…
Hi Ross,
we have added a 2.2 kΩ pullup and the problem persists. Would you think changing TLK106 to DP83822 will make an improvement in terms of noise immunity.
Thanks!
Hi Yacob,
OK, that was the first thing I saw was an issue. I'd like you to check the following items.
1. Look at timing of input reference clock PHY_2_CLK. If PHY_2_CLK is not stable when the TLK106 power comes up, you may need to apply a RESET…
Part Number: TLK106
We are using the TLK106 on two different hardware and are now having a problem with the link detection of the PHY when forcing 100Mb/FD. When the PHY is switched to this mode most times no link is detected and sometimes the link…
Other Parts Discussed in Thread: TLK106 Our customer has a question about TLK106. I'm posting the question for the customer:
++++++++++++++++++++++++++++++++++++++++++++++
We would like to use COL(Pin#29/COLLISION DETECT)signal as LINK-ON status signal…