Part Number: TLK106L Other Parts Discussed in Thread: TLK106 , DP83822I In my design I use TLK106L in RMII connection. I have a "not stable" behaviour during ping test between my board and the Personal Computer I use for test. Please note that…
Part Number: TLK106L Our application implements a Powerlink interface, with the following characteristics:
FPGA, Cyclon V, with Powerlink IP
two Ethernet posrts with TLK106L, both configured in RMII mode
One oscillator @ 50MHz configured as suggested…
Other Parts Discussed in Thread: TLK106L , TLK106 Hi,
I have a question about TLK106L polarity.
In customer board, output of link pulse was inverse polarity signal(TD+/TD-).
(They checked the signal from RJ45)
The customer are using default setting of Control…
Other Parts Discussed in Thread: TLK105 , TLK105L , TLK106L , TLK106 Hi TI team,
I am trying to figure out the differences between the TLK106 and TLK106L ethernet phy. (should also be valid for TLK105 and TLK105L)
Parametric search and datasheet dont yield…
Other Parts Discussed in Thread: TLK106L , DP83640 Dear Sir
I have some question about TLK106L
1.Fast Link Down Modes :
What's this feature benefit ? Is it mean if I meet some problem just like signal or energy loss ,TLK106L could Drop link from 100Mbps…
Hi Akash,
My apologies for the confusion, you are correct that the pinouts of the TLK110 and DP83822 do not match. The app note I linked discusses a back-compatible pin-to-pin replacement between the 822 and TLK105, TLK106, TLK105L, or TLK106L. Are you…
Part Number: AM6442 Other Parts Discussed in Thread: DP83869 , TLK105L , TLK106L
Hi,
We are planning to use the AM6442 processor from the Sitara series in our design which should support 1G Ethernet and the different industrial Ethernet protocols such…
Part Number: DP83822I Other Parts Discussed in Thread: SYSBIOS , TLK105 , , TLK105L , TLK106 , TLK106L
Hello.
If TLK105LRHB software applied to DP83822IRHBR, Will DP83822 IRHBR behave the same as TLK105LRHB? I am wondering if I can diversion the TLK105LRHB…
Part Number: TMDXIDK5718 Other Parts Discussed in Thread: TLK105 , TLK105L , TLK106 , TLK106L , AM5718
Hi,
In TMDXIDK5718 , TLK105 is used as the 10/100 Etherent PHY chip for PRU-ICSS.
DP83822 datasheet states "" pin-to-pin upgradeable option for…