Other Parts Discussed in Thread: TLK111 Hi, I'm trying to do the following:
a) delay power consumption of the TLK111 until my board has powered up (and negotiated for more power from the USB host).
b) use the SW_STRAP feature to avoid having to add…
Other Parts Discussed in Thread: TLK111 Hi,
I have the following questions:
Does CLKOUT (pin 25) need to be terminated in any way to avoid emission problems? It is a 25MHz clock
Is 4.87k critical for RBIAS (pin 24)? Will 4.75k or 4.99k work?
How is TX_ER…
Hello Pratik,
We don't have driver for PHY KSZ8081. You can use the drivers for dp83640 and Tlk111 as start point to develop your own driver for KSZ8081 PHY. dp83640.c and tlk111.c are generated by HALCoGen.
Hello,
Please use the following link to post any question regarding DP83882
https://e2e.ti.com/support/interface/f/138
I noticed that you made modification to HL_mdio.c. Does the original code get the same issue?
Do you get the same issue on TI HDK?
…
Part Number: RM57L843 Other Parts Discussed in Thread: DP83630 , TLK111 , DP83640 , HALCOGEN Dear Everyone,
I've just noticed that in the HALCoGen in the EMAC tab there is DP83640, TLK111 and Custom. But on the hardware after I inspected it, there is a DP83630…
Hi,
Yes, the TLK105L, TLK105, TLK106L, TLK106, TLK110, TLK100, TLK111, DP83848, DP83620, DP83630, DP83640, DP83849, and our very new DP83822 all support EtherCAT.
Please see the EtherCAT PHY Selection Guide:
Kind regards,
Ross
Part Number: TMS570LC4357 Other Parts Discussed in Thread: TLK111 , DP83640 , HALCOGEN
Tool/software: Code Composer Studio
Hi,
I am trying to use lwIP and FreeRTOS in a project. I tried it manually with the guidance of sources below. Also, I searched lots…
Other Parts Discussed in Thread: DP83630 , TLK111 , DP83640 , DP83640SW-LIB Can DP83630 be an IEEE 1588 master clock device? If not, are there other devices supporting it?
DP83630 supports the Precision Time Protocol (PTP). TLK111 also supports it. Can TLK111…
Part Number: TMS570LC4357 Other Parts Discussed in Thread: TLK111 , DP83640 Tool/software: Code Composer Studio I'm trying to build active webserver demo application following this wiki . Demo application file I got from here, in this post .
The error…