Part Number: TLV1171 Other Parts Discussed in Thread: TLV761 , TLV1117 , , TLV757P Hi team:
pls advice the P2P next Gen of TLV117112DCYR, i see the TLV761 is the next GEN, but no 1.2V output version yet. can you help to update this ?
Part Number: TLV1171 Hi team,
I received a question below from my customer. Could you please help with the question below?
I was searching for a LDO with
Vin=5V,
Vout=1V2,
Iout=1A,
SOT223 package
to use in a exiting design as a replacement .
The…
Hi Sanjay Pithadia ,
Following your suggestions, my design will be like this:
1. 1.8V Fixed supply: Using LMZ34202 and TLV1171-1.8.
2. 5V at 2A Fixed supply: Using LMZ34202
3. -5V at 2A Fixed supply: Using LMZ34002
4. +/-100V about 0.6A Fixed supply: Be generated…
Part Number: TLV4112 Other Parts Discussed in Thread: TLV1171 , LM2991 , TPS795 I am not sure if this is a simple question (I am not very experienced with electronics).
I want to use the TLV4112 op amp in a circuit where it is going to pass high current…
Hi Scott,
TLV1171 datasheet specifies Output current limit minimum = 1.1 A. When you apply the load current > current limit, the current limit activates and the Vout decreases as shown in your scope shot. After a period of time, the junction temperature…
Other Parts Discussed in Thread: TLV1117LV , LM1117 , TLV1171 Hi everyone,
Please let me know the thermal shutdown temperature of LM1117. I suppose that it should be 165degC (increasing) and 145degC (decreasing) which is specified at similar devices such…