Part Number: TLV1704 Hello,
I am using TLV1704AIPWR in our schematic with VCC 20VDC. Please help me to figure out the minimum and maximum input current requirement for TLV1704AIPWR.
Thanks,
Kiranjit
Part Number: TLV1704-SEP Hello - I have reviewed the reliability information on-line ( https://www.ti.com/quality-reliability-packaging-download/report?opn=TLV1704AMPWTPSEP ), but I cannot find the thickness of the gold in the leads. What is the thickness…
Part Number: TLV1704-SEP I want to check for this part TLV1704AMPWTPSEP , if it has a cavity inside, to see if we need to do a PIND test or not.
Please advise,
Thank you very much,
Salwa
Part Number: TLV1704-SEP Other Parts Discussed in Thread: TLV1701 Hello,
I would be interested to get the additional data on the open collector saturation voltage which you talk about:
"I have some data that I can't share publicly at this time. I'll contact…
Part Number: TLV1704-SEP We only specify the nominal leakage at room temperature (70nA) in the Nov2018 revision of the datasheet.
Do we have any guidance on the maximum leakage current that would be expected over process and the full temperature range…
Part Number: TLV1704-SEP Other Parts Discussed in Thread: TLV1704 , LM339 The Layout drawing shown in Section 10.2 of the data sheet has the labels for CH1 and CH2 swapped from the pinout drawing in Section 6. I assume the drawing in Section 6 is correct…
Part Number: TLV1704 Team,
I am seeing the negative input of a TLV1704 comparator can go about 10mV below ground in our application, while the positive input stays toward the middle of the common-mode range. The datasheet mentioned that the TLV1704 prevents…
Part Number: TLV1704 Other Parts Discussed in Thread: LM139 , LM239
Referring to above image, My supply voltage is different(+24V), I want to make Vout compatible to microcontroller interface(+3v3). can i connect pullup resistor to 3v3, so that i can…
Part Number: TLV1704 When looking to device mass of all TLV1704 (including SEP device) are not consistant
TLV1704IPWR is 80.7mg when all others are 57.1mg
SEP model is 115mg
are these number valid ?
is there a way to download the material declaration…
Part Number: TLV1704-SEP Hello,
Is there any data for SEL above 43 MeVcm2/mg and until 60 MeVcm2/mg?
Also, do you have any SET characterization?
Regards,
Beatriz