Part Number: TLV1805 Hi Team, I`m using TLV1805 in AC EV charger for control pilot signal, but I want to implement an isolated Control pilot signal. Please, suggest us with the suitable solution.
Thanks Tarun Kumar
Part Number: TLV1805 Other Parts Discussed in Thread: TLV4051 , TLV4041 , TL331 , TLV7011 Hi Team,
The main power input in my design is 12V. I need to monitor this 12V power and generate the PGOOD signal using a comparator with hysteresis.
The comparator should…
Yes, the problem seems to be solved. The sparking by connecting PCBA's together causes the TLV1805 to break. An TVS over the supply voltage and one over the output does the trick.
Thank you very much for the support!
Part Number: TLV1805 Dear Team,
what is the max voltage at OUT pin at high-z state? At supply voltage of 3.3V (V- = 0V)
It is planned to pull-up OUT pin with a 10-100k pull-up to 18V
Power-supply of TLV is only present AFTER the 18V
Datasheet 6.1 doesn…
Part Number: TLV1805-Q1 Hi there,
I've just finished my design but now this chip is out of stock.
Are there alternatives to this chip?
Kind regards,
Laura
Part Number: TLV1805 Dear TI Team,
We are planning to use TLV1805 as an oscillator (in the MHz range). TLVs' datasheet does not contain a design procedure to use TLV as an oscillator.
The link from its datasheet leading to an oscillator design (Engineers…
Part Number: TLV1805 Hi, I've a fixed current source of 500mA and a variable voltage supply between 0-20V AC. I'm aware of FET Vgs but that's out of scope for this question. Generally the voltage will be somewhere in-between and I'm not using PFC below…
Part Number: TLV1805 Hi,
I downloaded the TINA simulation for the TLV1805.
When I simulate the rise/fall times I get approx. 10 times larger values than the datasheet.
With a capacitive load of 1200pF I simulate ~1000nS, but the datasheet states ~100ns…
Part Number: TLV1805 I work for Lockheed Martin and we can't load 3rd party software without getting permission from the IT mafia. Can you please send me the .txt of the model for the TLV1805. I want to add it to my LTspice simulation.