Part Number: TLV2314 Tool/software: Hi expert,
I posted my question three days ago, but it could be deleted. So I post it again.
There is a probabilistic failure of the chip, and the phenomenon is that the output remains at 4.7V all the time, even…
Part Number: TLV2314 General Purpose Amplifier 2 Circuit Rail-to-Rail 8-VSSOP
After decapsulation, the die marking "5360" does not leading to a firm conclusion or result based on the part number (TLV2314IDGKR).
Part Number: TLV2314 Other Parts Discussed in Thread: OPA2314 , TLV314 Hi,
May I know where I can obtain the unencrypted Pspice model for TLV2314?
Thanks,
Christina
Hello User,
Even in the sample waveform, the output is a little smaller than expected and is adding distortion (mismatches between input and output). The output peak to peak is about 7.5 times the input, but the programmed gain is 10. Some of the input…
Part Number: TLV2314 Other Parts Discussed in Thread: LMV358 , TLV342 Hello Team,
I am looking for a dual OPA that keeps the output voltage near 0V during Vcc ramp when configured as a difference amplifier and input voltage of 0V.
Configuration for…
Hi Joe,
You can use the information for the OPA2314 which shares the same footprint as the TLV2314. See link below:
https://webench.ti.com/cad/cad.cgi?partno=OPA2314
Part Number: TLV342 Other Parts Discussed in Thread: OPA2310 , OPA2383 , OPA2314 , TLV341 , TLV2314 Hi. I designed the TLV342 into a design in 2023, and it's running in volume. At first we noticed that we were seeing pretty consistently about 88uA per…
Hi Jason,
a total gain of 270 means a gain of factor SQRT(270) = 16.4 per stage. For a bandwidth of 20kHz the OPAmp should have a minimum gain reserve (loop gain) of factor 10 at 20kHz. Combined with a gain of factor 16.4, an OPAmp with an open loop…
Part Number: TLV9002 Other Parts Discussed in Thread: TLV2314 , OPA2314 , TLV9052 Dear,
I'm trying to use your TLV9002 instead of OP2314/TLV2314 for our product. Op-amps are used for transimpedance amplifiers. And Both operate by same circuit and operation…