Other Parts Discussed in Thread: TLV2370 Hi - sorry, got some questions on TLV2370 shutdown. I'm aware that its a older product and answers may be difficult but I have a customer asking
Firstly what the threshold voltage for the shutdown pin - bit…
Hugo,
There is no data sheet rating for TLV2371. I did find ESD sample data for TLV2370, dated 3/15/2001. TLV2370 is a TLV2371 except it has an extra pin for shutdown. HBM was tested up to 4kV and passed (2kV was the highest test voltage for other TLV237x…
You're welcome. If I come up with any other suggestions I'll follow up. Please post back if you determine that the TLV2370 won't meet your needs.
Best,
Paul
CK Ho,
TLV2370, OPA743 and OPA191 are few options with high voltage (>12V) supply capability, comparable specs and RRIO. But these are not directly P2P compatible with LM321. You will have to swap your Pin1, Pin3 and Pin 4.
Lets us know if this is…
Hi Phil,
Please see the attached TLV2370 Aol and Zo graphs. The TLV2370 is a single op amp variation on the TLV2372 and theIR Aol and Zo will be the same. These graphs are from recent measurements taken by our staff. Ignore the upward spike in the gain…
Other Parts Discussed in Thread: TLC251 , TLV2370 , TLV2460 In Single-supply mode with VDD=12V, Vdd- at GND, and set for "High-bias mode", What output current can this opAmp drive a 10K load to ? Can it drive a 10K load to 10v at 1mA ? Doesn't look…
Depending on application and performance "care-abouts" the TLV27x family CMV includes GND as well as many of the TLV devices at a single supply of 12V. for RRIO, the TLV237x family should be reviewed (CMV 0 to Vdd)
http://focus.ti.com/lit/ds…