Part Number: TLV2474 Other Parts Discussed in Thread: TLV2472 , TLV274-Q1 , TLE2071A Hello e2e,
Quality and Reliability folder states to look in the datasheet for ESD, HBM CDM, details for the following devices but details are not in the datasheet.
TLV…
Hi Ore,
Thanks, but checked that OPA2333-Q1, automotive device has max 125 degree spec.
Could you answer these questions below?
1. Check schematic for TLV2474-Q1 and see if there's anything to revise?
2. Check TLC2274EPWRQ1 is fine for pin 2 pin…
Hi Paul,
I am seeing the clipping in the R-R TLV2474s itself, I stopped using the LMV344 because of the temperature problem. Got rid of the 150k and made the input resistor 8.5k to get the slight amount of gain for oscillations.
Either way, I am now using…
Hello Yeon,
Yes, TLV2474x-Q1 can have different pattern regardless TLV2474 A QDRG4Q1 or TLV2474 QDRG4Q1
For any op amp, the lead frame can vary. Check the reel label for the county of origin. Even in same country, lead frame may vary.
Other Parts Discussed in Thread: TLV2474 , TINA-TI Greetings! My name is Gilberto and i am a graduation studdent of automation engineering from Brazil. I am having trouble with the understanding of the function and sizing of the resistors Rg and Rf for the…
Hi Shambhulingayya,
thanks, it works now!
Nevertheless, I see lots of distortion with the OPA4227, mainly at the cosine output. With the TLV2474 the distortion is much lower, nearly invisible. So, I aggree with Thomas, that you should give the TLV2474…
Other Parts Discussed in Thread: TLV2474 Hello,
I am trying to generate 150Khz using bubba oscillator. I first tried with the 60 Hz example and changed the values. But it didnt help. I then referred to the design of the following post ( http://e2e.ti…
Other Parts Discussed in Thread: TLV2474 , OPA365 , TLC555 6332.OpAmp_Oscilitor_slyt164[1].pdf.pdf Dear all,
I try to simulate a Bubba oscillator in TI-TINA. it is strange that the circuit does not work. i don't know why. wish for your suggestions. thanks…