Part Number: TLV3012-Q1 Other Parts Discussed in Thread: TLV3012TLV3012AQDCKRQ1
TLV3702QDRG4Q1
TL331QDBVRQ1
For these three Comparators, the ESD ratings have been omitted from the most recent datasheets, even though the Qualification Summary page for…
Part Number: TLV3012 Other Parts Discussed in Thread: TLV4021 , LMP7300 , INA206 , TSM102 , LMV7231 Hello,
I'm considering using TLV3012-Q1 in a design. I do not have any issues with it so far, but I did notice it is a bit older. Is this the best part TI…
Part Number: TLV3012 Does TLV3012 require a series resistor in-line with the inputs to limit the current if inputs ever go beyond the supply voltage? Don't see this info in the datasheet.
Thanks
Viktorija
Part Number: TLV3012 Other Parts Discussed in Thread: TLV7031 , TLV6703 , TLV7011 Hellow,
I am testing the TLV3012 at low temperature (-40C) and i found that the internal voltage reference was decreasing. At +55C down to -30C the voltage reference stable…
Part Number: TLV3012 Hello,
I am using the TLV3012AIDCKT comparator of TI.
We checked the comparator at over temperature and we found that the propagation delay(tPHL) is more than 12.5usec when freezing the board.
Refer our schematic, I place probes…
Part Number: TLV3011 Other Parts Discussed in Thread: TLV3012-EP , Dear Sir,
Our Base part is TLV3011AMDBVREP (Open-collector) & new recommended Part is TLV3012-EP series (Push-Pull), so is this part is OK to use in our existing circuit.
Is this difference…
Other Parts Discussed in Thread: TLV3012 , TLV3012-EP Good morning,
we are testing TLV3012 at low temperature -40°C and some problem happened during test.
Testing condition: Supply voltage 5Vdc, power up circuit at -40°C, application railways. Climatic…
Other Parts Discussed in Thread: TLV3012 I am searching for .LIB and .OLB files for TLV3012. I tried searching here: http://www.ti.com/product/tlv3012, but the ZIP file did not have anything.
Hello Collin,
Would it mean that even for open-drain output comparators like TLV3011 or LM2903, the outputs are diode clamped to theirs V+ and V- pins ?
That would imply that I couldn't supply the pull-up resistor output with a higher voltage than the…
Other Parts Discussed in Thread: TLV3012 The TLV3012 is rated for up to 10nF capacitive load on the reference terminal.
What is the minimum output series resistance that I need to drive 100nF load without oscillation?
Peter