Part Number: TLV314-Q1 Other Parts Discussed in Thread: TLV314 Hello,
To read the current of each phase in motor drive application, shown in figure 1 (Ia, Ib, Ic), an offset voltage of 1.65V is created using TLV314.This is due to the fact that the current…
Hi Kevin,
It's been several weeks since we heard back. I'm going to assume that this issue has been resolved and close the thread.
Best Regards,
Robert Clifton
Part Number: OPA335 Other Parts Discussed in Thread: TLV314 , Hi,
I'm using the circuit below to sense the DC BUS voltage, ADC_Udc=(135/23919)*Udc, ADC_Udc is fed to the ADC of MCU.
The DC bus voltage ranges from 50V to 500V.
I compare the actual DC…
Part Number: TLV314 Other Parts Discussed in Thread: TINA-TI Hi,
I have one MFB circuit built using TLV314.
I am assuming that spice model of TLV314 doesn't include offset voltage.
In case of steady state, input will be attenuated by Rf/Rin which…
Part Number: TLV314-Q1 Hi team,
As one of reliability information, it seems the customer would like to know what the behavior of TLV314-Q1 is when adjacent pin is shorted. Do you have any documents, materials or blogs that shows the behavior at short of…
Hi Russell,
I'm assuming you are looking for the TLV313-Q1 Pin FMEA. We do not have the documentation for the TLV313-Q1 Pin FMEA online but the Pin FMEA for the TLV313-Q1 will be identical to the TLV314-Q1 as long as the pin outs of the packages you are…
Part Number: LM258 Other Parts Discussed in Thread: TLV314 Hi team,
Below is LM258 SCH. We can see, if it work, LM258 U1 is output 0.5V. But actually it output 0.53V. When remove R492, it output=0.5V normally.
Keeping R392 in the board, I let U2 , U3…
Hi Vijay,
There are some big differences between the two devices:
Slew Rate:
LF356 = 12V/us
LF357 = 20V/us
GBW:
LF356 = 5MHz
LF357 = 20MHz
Do you know what the design requirements are? Can the customer use the TLV314 or TLV316 instead? They will come…
Part Number: TLV2314 Other Parts Discussed in Thread: OPA2314 , TLV314 Hi,
May I know where I can obtain the unencrypted Pspice model for TLV2314?
Thanks,
Christina