Part Number: TLV3491 Hi,
The below is the schematic diagram, the VDD=48VDC, this design is used for the check if VDD is more than 52.5V, and TLV3491 is output the high to the MOSFET(Infineon IRLS4030) when VDD more than 52.5VDC;
The 5VDC and 2.5VDC are…
Part Number: TLV3491 Other Parts Discussed in Thread: TLV7011 Hi Experts,
Good day.
We don't see the start up time for the comparator TLV3491 in the datasheet.
Can you help us to figure out what it is?
Thank you.
Regards, Archie A.
Part Number: TLV3491 Other Parts Discussed in Thread: TLC271 , TLV4062 like to know the input impedance on TLV3491
Cannot find on datasheet when for example TLC271 datasheet provide info (typ 10power12 ohm)
regards
Part Number: TLV3491 Other Parts Discussed in Thread: TLV7031 Hi,
We are planning to power the device from a +3.3V supply, however, we will be driving inputs up to +/-15V. If I limit the current going through the internal ESD diodes to 0.1mA using a 150kΩ…
Part Number: TLV3491 Hello,
I'm working on a design with a TLV3491AID as a simple DC comparator circuit. The supply for it is still in flux however I noticed in the datasheet for it that the absolute maximum supply voltage is 5.5V and the recommended…
Part Number: TLV3491 hi
Can I check do you have conflict mineral report template for version 4.2? If yes, can you send it to me for the device: TLV3491AIDBVRG4
Best regards,
kpk
Hi Hollis,
I made calculations to determine the hysteresis voltage switch points initially assuming an ideal comparator and the resistor values used in your circuit; noteably with the 22 MEG feedback resistor. The ideal comparator's output would switch…
Hi Chuck,
I only tested with one tlv7031 and with one tlv3491, and de skew of both was similar.
When i tested with the voltage divider using two 470k and after with two 100k i noted some significant change if i remember(both tests with tlv3491 only). …
Part Number: TLV1701 Other Parts Discussed in Thread: TLV3401 , TLV3491 Hi Expert,
Could you please let me know the Propagation delay at overdrive=2mV
Thanks
Muk
Part Number: ADS1298RECGFE-PDK Other Parts Discussed in Thread: MSP430G2121 , TLV3491 , ADS1298R Hello,
We are working on ADS1298R we has Ref. Board now we want to design custom hardware so we have some doubt in the Reference design The MSP430G2121(MCU)…