Okui-san,
The next step up in higher output current would be the TLV4112. The TLV411x family is capable of output currents in excess of 300 mA, with V+ of 5 V. The power and thermal considerations in data sheet pages 13 to 16 must be carefully observed…
Hello Atsushi,
The equivalent graph to AZV358 Fig 14 is figure 8 on the LMV358-N or Fig 15 on the LMV358 datasheets.
For the AZV358, at 25mA, the output is just under 2V from the rail...so you only have 0.7V of swing left.
The LMV358-N most likely it…