Part Number: TLV803 Hi team,
I’d like to double check the spec of Supply current in datasheet. Can you confirm below questions?
For the max current of Idd (at Vdd=6V),
-. Is it within 30uA, regardless of external pullup resistor size?
-. Is it within…
Other Parts Discussed in Thread: TLV803 I'm using a TLV803SDBZT for a magnetic sensor application and the component (unpowered) give off magnetic interference (around 5000 nanoTesla) that I'm trying to get rid off. I've been able to find non-magnetic…
Dear Sirs:
I have a condition at 95 degree C ambient where a TLV803S is connected to the reset pin 2 of a Freescale MC5684565 uC with a 10K pull up to 3.3v and a 0.1uF pull down to ground which some times lock to a 600mV level.
If I bring the temperature…
Hi Tom,
The digital rail should be brought up first. After that, simply sequence the power such that rails come up in an increasing order. See example below for this device:
DVDD18 ⟶ All other 1.8V rails (in no particular order) ⟶ All 3.3V rails (in no…
Hello Ray,
I would like to ask some doubt regarding the SMPS.
1A. What components do I need to change if I want to change the Switching MOSFET? Please advise.
1B. Should I consider other MOSFET's rise time, fall time, input capacitance and gate charge…
Hello,
Unfortunately we do not offer dedicate model for this version. We have models for the open0drain versions of this device. Hope that help.
TLV803 data sheet, product information and support | TI.com
Hello Jake,
Thanks for your comment. I used a simple rectifier similar to Figure 5 in slva594 as quick prototype to test the circuit performance.
The rectifier and voltage divider works fine without connecting it to TLV803. The phenomena happens when I the…
Hello Brian, thanks a lot for your answers. Here is what I can input: 1: Upstream port is J4 indeed. I put 100nF AC caps on both lines, as shown on the inserted pic. I don't remember seeing 330nF on the datasheet for upstream port implementation ? Did…
Part Number: AM4372 Other Parts Discussed in Thread: TIDEP0020 , TLV62565 , TLV62080 , TLV702 , TLV803 , TLV62568A , TLV743P , TLV740P , TLV803E Dear Champs,
We are trying to suggest discrete power rails for AM4372 based on below ref. design(TIDEP0020).
https…