Part Number: TLV9102 Tool/software: I have questions about TI components for my design and will appreciate your help.
TLV9102:
This is my scheme. The datasheet mentioned that the common voltage can’t exceed VCC+0.5V. What will happen if, for…
Part Number: TLV9102 Other Parts Discussed in Thread: TLV9032 , , TLV9022 U13 (TLV9102) is a rail-rail OPAMP. Do we need to use comparator? TLV9022/TLV9032. IO_SENSE is compared with a Fixed value, to output logic signal.
Part Number: TLV9102 Hi team, Section 7.3.5 of the datasheet contains descriptions for use in V(+)-2V applications. However, the recommended operating range is V(+)-0.1V. Does this mean it cannot be used in Rail-to-Rail applications? Could you tell the…
Part Number: TLV9102
Tool/software:
Hello all,
I hope you're having a nice day.
Lately I have been sketching this constant current circuit that uses the TLV 9102S, a dual operational amplifier. The idea is to supply a constant current (1 mA) through…
Part Number: TLV9102
Tool/software:
Hello all, I hope you're having a nice day.
I'm planning to use TLV9102S dual op-amps in a kind of multiplexing application where an op-amp must be placed in shutdown mode. This application requires the output…
Part Number: TLV9102 Hi,
I'm using the TLV9102 for various industrial AIO drivers. These drivers will not be disabled at any time.
Because of this, I want to consistently (and clearly) disable the SHDN (Shutdown) function of the operational amplifier…
Part Number: TLV9102 Other Parts Discussed in Thread: ADS8862 ,
Dear Technical Support Team,
I have Output Oscillation issue with 2700pF on output.
The configuration is buffer for ADS8862.
When Riso is inserted on output, then output seems to…
Part Number: LPC662 Other Parts Discussed in Thread: LMC6082 , TLV9102 Hello,
My customer has to redesign the circuit using LPC662 to LMC6082 due to the EOL issued. From the PCN it doesn't get much detail on electrical differences. Has your team done…
Part Number: TLV9102 Other Parts Discussed in Thread: LMC662 , LMC6061 , LMC6081 , LMC660 Dear Team,
May I know the I/P resistance of TLV9102.
In TI website I can see that TLV9102 is a replacement for LMC662.
LMC 662 has I/P resistance grater…