Part Number: OPA2991 Other Parts Discussed in Thread: TLV9102 , Hi What is the procedure to measure the CCMR of 130db on this amp? Thanks for your help
Hey Hailiang,
The thread has been transferred back to GPAMPS to find a low cost solution. If the Vos specification can be moved to 1.5mV, then there are three options less than $0.50/ku, the TLV9002 (low voltage), TLV9102 (mid voltage), OPA2990 (high…
Part Number: TLV9062 Other Parts Discussed in Thread: TLV9302 , OPA2990 , TLV9042 , TLV9352 , TLV9052 , TLV9152 , OPA2991 , TLV9102 , LM358B , TLV9002 Hello,
I was reviewing this E2E post which states that any of these operational amplifiers could also be used…
Part Number: TLV2171 Other Parts Discussed in Thread: TLV9102 , OPA2991 , OPA2990 , TLV9152 , OPA2244 , TLV9042 , TLV9151 Hi team,
My customer use TLV2171 to sense battery voltage, and they want to decrease the TLV2171 Iq consumption during the off-work status…
Hello Ron-san,
Thank you for your quick reply.
> The PS will be the same 8 pin pinout
I understand both D(SOIC) and PS(SO) are 8 pin package with different dimension as shown on page 41 for D(SOIC) and 44 for PS(SO). Would you update the datasheet to…
Other Parts Discussed in Thread: TLV9162 , TLV9152 Battery test applications require voltage accuracy of 0.01% or 100 ppm of the full-scale range after system calibration. General-purpose amplifiers with 1 µV/ °C input offset drift can easily meet…
Hey Cici,
I opened your archive project and also ran into some convergence issues. These are the steps I took to remedy:
1. Turn on autoconverge (this is located in Simulation Settings -> Analog Simulation -> Auto Converge -> Select All) 2. Remove…
Part Number: TL062 Other Parts Discussed in Thread: TLV9102 , TLV2372 , TLV272 I need the fet inputs for high input impedance. will the TLV9102 fit this criteria?
Part Number: TLV9302 Other Parts Discussed in Thread: TL082 , TLV9102 , TLV9352 , , TLV9152 Hi,
my customer was using TL082 to sense the output current of an PSFB converter.
TL082 is used to sense the current with a shunt resistor placing at ground side(R27…
Part Number: TPS65132 Other Parts Discussed in Thread: TLV9102 , TPS61391 , Hello there,
I have a few questions regarding the TPS65132 - I have described my goals and questions follow.
Aim: To generate (i) dual rail voltage supply of +/-5V for two summing…