Part Number: INA381 Other Parts Discussed in Thread: TLV9152 , , LM2903 , INA180 , TLV3231 Tool/software: Hi team,
I'm looking for op amps and comparators that enable high-speed overcurrent detection for compressor motor. Could you tell me the fastest…
Part Number: MC1458 Other Parts Discussed in Thread: CC1190 , TL072H , TLV9152 Tool/software: Dear Sir,
We recently purchased the IC, part number MC1458DR , through the Texas Instruments online portal under order no. T05640968
We are facing the following…
Part Number: TLV9352 Other Parts Discussed in Thread: LM358B , , TLV9102 , TLV9152 Hello, LM358B accepts the input signal voltage exceeding V+ up to 40V. My customer is looking for a 2ch opamp like it with lower offset voltage drift and lower offset current…
Part Number: TLV2372 Other Parts Discussed in Thread: TLV9152 Hi,
just want to check on next gen of TLV2372. and it's better to be p2p. I see on roadmap there is TLV910x, is it the right part? Thanks.
BRs
Given
Hello Daniel,
This device is a custom part and does not have a public orderable. please feel free to email us for further information.
The best alternative to maintain performance is the TLC2272A-Q1 . The next generation of the device is the TLV9152…
Other Parts Discussed in Thread: TLV9102 , TLV9101 , TLV9162 , TLV9151 , TLV9161 , TLV9152 Hi team,
do we have device support below request?
device select function;
Channel numbers:1or 2;
VOUT range:0~12V;
VIN range:0~5V;
shutdown current…
Hi Sumeet,
Sumeet Patil said: I am looking for a direct pin to pin part replacement of LMC6482IN_NOPB, which can operate at +/- 15V
The equivalent and p2p replacement may be TLV9152 .
Here is the comparisons. However, either one is able to supply…
Part Number: TLV9102 Other Parts Discussed in Thread: TLV9152 The TLV9102S is available in the package X2QFN (10).
On the top page of the datasheet in the table “Device Information” the Body Size (nom) of this package is listed as “1.50 mm x 1.50 mm…
Part Number: OPA2374 Other Parts Discussed in Thread: TLV9062 , MCP6292 , TSV912 , TLV9152 , OPA2323 When testing this series of op-amp in an integrator circuit we discovered some significant coupling between the input and the output feedback. This phenomenon…