Part Number: TM4C1233E6PM Hi, I'm building a datalogger for IoT with the TM4C123.
I have some questions:
1) how to set the RTC time?
2) How do I get date and time when I compile my code and update the Date/time automatically in my system.
3) Is there…
Other Parts Discussed in Thread: TM4C123GH6PM , TM4C1233E6PM Hi Sirs,
From the datasheet, found that there are USB and CAN MAC different between these 2 parts.
May I know what is different for these 2 parameter?
TM4C123GH6PM can be programmed firmware…
Register 2: Device Identification 1 (DID1) reads 1003602C which indicates Bit 1:0 QUAL 0x0 Engineering Sample (unqualified). The chip marking does not even have a TI Logo on it. How comes that you get unqualified stuff without being informed? After the…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Hello George,
Thanks for your replay.
Regarding the second warning test case:
Compiler version: TI v16.9.6.LTS [TI v18.1.1.LTS]
Build output:
**** Build of configuration Debug for project AutosarCanStack ****
"C:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 8…
Thanks George,
compiler version: TI v16.9.6.LTS [TI v18.1.1.LTS]
Here is the build console output:
**** Build of configuration Debug for project AutosarCanStack ****
"C:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 8 arch/arm-cortexM4/drivers/Can.obj -O …