Part Number: TLC555-Q1 Tool/software: Hi Team, Request you to please provide Electrical Characteristics at VDD = 10 V, which will help in our design. Regards, Vamsi Bankuru
Part Number: ALM2403-Q1 Other Parts Discussed in Thread: ALM2402F-Q1 , Tool/software: We want to detect the current consumption on each output stage. This can be done through a shunt resistor connected on pins 10 and 12, then monitored through a current…
Part Number: DP83TC812S-Q1 Tool/software: I would like to ask how to send a WUP to the DP83TC812. WUP is not an Ethernet packet; it seems to be just a frame at the OSI Layer 1 (physical layer), not an Ethernet packet at the MAC layer
Part Number: DP83TC812S-Q1 Tool/software: Hello, the Typical TC-10 application block diagram is as follows. May I ask if I can turn off the power to VDDA/VDDIO/VDDMAC in TC-10 mode? Do you have any recommended VREG chip models?
Part Number: TPL0401A-10 Other Parts Discussed in Thread: DAC43701 Hello team,
the customer has asked a replacement solution for their currently used Single Digitally Controlled Potentiometer ISL95810UIU8Z-T (Rensas), .
TI does not have a direct pin-to…
Part Number: LM5176-Q1 Tool/software: HI everyone,
We have faced few below mentioned problems with LM5176-Q1 when we tested With PCB. The schematic attached for your reference
It is not boosting 24 V from 9 V input but it is working from 10V. However…
Part Number: TL431-Q1 Tool/software:
Dear TI Team,
I looking for calculation of worst case voltage deviation of TL431B-q1 in the temperature range 10°C to 50°C. Full temperature range shows 34mV max deviation.
Thanks!
Part Number: TMS320F280038C-Q1 Tool/software: I have installed CCS12.8 and connected an XDS110.
I can use xdsdfu -e and get
USB Device Firmware Upgrade Utility Copyright (c) 2008-2019 Texas Instruments Incorporated. All rights reserved. Scanning USB…
Part Number: TPS22995H-Q1 Other Parts Discussed in Thread: TPS22999 , TPS22954 Tool/software: Team,
do we have an alternative in our portfolio (or on roadmap) that is similar to TPS22995H-Q1 but has a QOD resistor of 10 Ohms?
Best regards
Part Number: LM5143-Q1 Other Parts Discussed in Thread: LM5143 , TDA4VH , LM25143-Q1
Tool/software:
Hi LM5143 Champ !
My customer would like to set input voltage range from 10~24V and maximum output voltage level is 3.3V since they believe the LM5143 seems…