Part Number: TPL5010 Hi Support,
According to datasheet the TPL5010 is reading the Rext resistance during the POR.
I want to change the Rext resistance during the TPL5010 operation without turning the power off and on again.
Is it possible?
If the answer…
Part Number: TPL5010 Tool/software: Hi Expert,
TPL5010's schematic as below, and RSTn is pull up, the DONE is always feeding the dog.
The WAKE pulses sometimes decrease to 2ms or 8ms from 20ms. I suspect that the problem is caused by the instability…
Part Number: TPL5010
Dear TI support,
I have one questions about datasheet of TPL5010.
In section "8.3.2 DONE" it can be read: "The DONE signal resets the counter of the watchdog only.". I thought, incorrectly, that each time the…
Part Number: TPL5010 Hello, I am using the TPL501010DDCR integration, but the timing I set for 5 minutes resets after 9 minutes at the earliest. I use 43k as timing resistor.
Part Number: TPL5010 Hi,
Please recommend a watchdog chip.
Temperature -40°C to 125°C
Low power consumption 35nA
Power supply 1.8v-3.3v
Reset pin: Output low
When resetting, a mos tube is needed to power off the mcu
No manual key reset required…
Part Number: TPL5010-Q1 Hello,
also in my application the IC power supply is 3.3V and I would like to pull the RSTn pin to +5V. The datasheet reports that the "input voltage at any pin" must be less than VDD+0.3V and it seems to include also the RSTn pin (even…
Part Number: TPL5010-Q1 Other Parts Discussed in Thread: TPL5010 Dear TI expert,
Customers use TPL5010-Q1 as the watchdog chip of the MCU, and at the same time connect the RST pin of the MCU to a reset IC, as shown in the figure below, there is currently…
Part Number: TPL5010-Q1 Hi,
I want to ask a question:
In the TPL5010-Q1 datasheet, the typical value of tRSTn width is defined as 320ms. What is the maximum value?
Because after the completion of VALID_RST, the software needs to give a DONE signal, and…
Part Number: TPL5010 Other Parts Discussed in Thread: TPS3852
Can I set something so that I can get the blue color result that I shows in the following picture ?
Is the TPL5010 can meet my requirement ? Or can you suggest another part that can help me…
Part Number: TPL5010-Q1 Hi team,
I have a question regarding TPL5010-Q1.
If I only utilize the timer function of TPL5010-Q1, don't use the watchdog function, what to do with the DONE pin? Will I still need input logic signal to this pin or leave it floated…